Solution
Downhole Force Measurement
Deviated and lateral wells render topside measurements of little value. Successful pump down services require accurate tool string tension readings, downhole, at the source.
Deviated and lateral wells render topside measurements of little value. Successful pump down services require accurate tool string tension readings, downhole, at the source.
The IPCD Pressure Compensated Downhole Load Cell is an accurate and reliable load cell that Interface has developed specifically for downhole tension and compression measurements in high temperate, high pressure well conditions. Featuring proprietary pressure and temperature compensation, precise tool string force measurements can be monitored real time through customer instrumentation.
Customer was able to control pumping forces on the tool string with incredible accuracy. Regulating this process ensured service success without the risk of tool pump off, avoiding a devastating and expensive fishing operation.
IPCD Pressure Compensated Downhole Load Cell
Customer Instrumentation
The IPCD Pressure Compensated Downhole Load Cell is integrated near the top of the tool string.
During pump down, the IPCD measures the tension between the cable head and the tool string.
Connected to the customer’s instrumentation, actual cable head tension is closely monitored across any variation of temperature or pressure.
Notifications